Keysight 89600 VSA .NET API
FrequencyVersusTimeChannel Class Members
See Also  Properties  Methods  Events
Agilent.SA.Vsa.Interfaces Assembly > Agilent.SA.Vsa Namespace : FrequencyVersusTimeChannel Class

Glossary Item Box

The following tables list the members exposed by FrequencyVersusTimeChannel.

Public Properties

 NameDescriptionMinimum SW Version
Public PropertyIsDisposedGets a value indicating whether the object has been disposed. If an object has been disposed any attempt to use it will lead to an ObjectDisposedException being thrown. (Inherited from Agilent.SA.Vsa.RemotableObject)—
Public PropertyMaxAnalysisPointsGets or sets the maximum number of analysis points allowed.  —
Public PropertyMaxAnalysisPointsAutoGets or sets a value indicating whether the maximum number of analysis points should be automatically determined.  —
Public PropertyResolutionBandwidthGets or sets the resolution bandwidth (in terms of ENBW) used to determine how to split the acquisition by.  —
Public PropertyResolutionBandwidthAutoGets or sets a value indicating whether the resolution bandwidth should be automatically determined based on the measurement span.  —
Public PropertyTimeStepGets or sets the time step used to calculate the overlap amount between blocks.  —
Public PropertyTimeStepAutoGets or sets a value indicating whether the time delta used to calculate the overlap amount between blocks should be automatically determined based on the measurement span.  —
Public PropertyWindowGets or sets the window function applied to the frequency versus time analysis.  —
Public PropertyWindowAutoGets or sets a value indicating whether the window should be automatically determined based on the measurement.  —
‡ This is the minimum 89600 VSA software version level needed to use this member.
Top

Public Methods

 NameDescriptionMinimum SW Version
Public MethodCreateObjRefCreates an object that contains all the relevant information required to generate a proxy used to communicate with a remote object. (Inherited from System.MarshalByRefObject)—
Public MethodForceRebuildKeyMapThis method is used to force a refresh of the key map. This is necessary in cases where the key mappings to the API objects change. This can happen when the index of an item within a collection is reflected in the key name, and an item is removed from the middle of a collection. (Inherited from Agilent.SA.Vsa.RemotableObject)—
Public MethodGetLifetimeServiceRetrieves the current lifetime service object that controls the lifetime policy for this instance. (Inherited from System.MarshalByRefObject)—
Public MethodInitializeLifetimeServiceObtains a lifetime service object to control the lifetime policy for this instance. (Inherited from Agilent.SA.Vsa.RemotableObject)—
‡ This is the minimum 89600 VSA software version level needed to use this member.
Top

Public Events

 NameDescriptionMinimum SW Version
Public EventPropertyChangedOccurs when a property value changes. (Inherited from Agilent.SA.Vsa.RemotableObject)—
Public EventPropertyInfoChangedOccurs when secondary information about a property, such as limits, changes. (Inherited from Agilent.SA.Vsa.RemotableObject)—
Public EventRemotePropertyChangedOccurs when a property value changes. (Inherited from Agilent.SA.Vsa.RemotableObject)—
Public EventRemotePropertyInfoChangedOccurs when secondary information about a property, such as limits, changes. (Inherited from Agilent.SA.Vsa.RemotableObject)14.00
‡ This is the minimum 89600 VSA software version level needed to use this member.
Top

See Also