Keysight 89600 VSA .NET API
IsPolynomial Property
See Also 
Agilent.SA.Vsa.Interfaces Assembly > Agilent.SA.Vsa Namespace > Graph Class : IsPolynomial Property


Glossary Item Box

Gets or sets a value indicating whether the curve fit polynomial is calculated.

Syntax

Visual Basic (Declaration) 
Public MustOverride Property IsPolynomial As Boolean
C# 
public abstract bool IsPolynomial {get; set;}
C++/CLI 
public:
abstract property bool IsPolynomial {
   bool get();
   void set (    bool value);
}

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 17.00

See Also