Keysight 89600 VSA .NET API
Graph Class Members
See Also  Properties  Methods  Events
Agilent.SA.Vsa.Interfaces Assembly > Agilent.SA.Vsa Namespace : Graph Class

Glossary Item Box

The following tables list the members exposed by Graph.

Public Properties

 NameDescriptionMinimum SW Version
Public PropertyDescriptionGets or sets a description string value to be drawn above the graph.  18.00
Public PropertyDrawShapeGets or sets how the result data's points are drawn.  17.00
Public PropertyIsAmplitudeNormalizedGets or sets a value indicating whether the resulting trace is computed with the response trace's amplitude normalized.  17.00
Public PropertyIsCompensateGets or sets a value indicating whether any compensation (time alignment, power level, and phase error) is enabled.  17.00
Public PropertyIsDataNamesAutoGets or sets a value indicating whether the stimulus and response data is automatically selected.  17.00
Public PropertyIsDisposedGets a value indicating whether the object has been disposed. If an object has been disposed any attempt to use it will lead to an ObjectDisposedException being thrown. (Inherited from Agilent.SA.Vsa.RemotableObject)—
Public PropertyIsPhaseCompensateGets or sets a value indicating whether compensation uses the phase of stimulus and response data.  17.00
Public PropertyIsPhaseCompensateAutoGets or sets a value indicating whether IsPhaseCompensate is determined from the center frequency of the stimulus and response data.  17.00
Public PropertyIsPhaseErrorCompensateGets or sets a value indicating whether phase error compensation is enabled.  17.00
Public PropertyIsPhaseErrorCompensateAutoGets or sets a value indicating whether phase error compensation will use the default filter length.  17.00
Public PropertyIsPolynomialGets or sets a value indicating whether the curve fit polynomial is calculated.  17.00
Public PropertyPhaseErrorCompensateSpanPercentGets or sets the phase error compensation filter bandwidth as a % of span.  17.00
Public PropertyPolynomialOrderGets or sets the curve fit polynomial order.  17.00
Public PropertyResponseDataNameGets or sets a value which selects the response data (the same names as used in Trace.DataName).  17.00
Public PropertyStimulusDataNameGets or sets a value which selects the stimulus data (the same names as used in Trace.DataName).  17.00
Public PropertyTimeAlignPercentGets or sets the search length (percent) to align the input time data.  17.00
Public PropertyTimeReferenceGets or sets how the result data points time reference.  17.00
‡ This is the minimum 89600 VSA software version level needed to use this member.
Top

Public Methods

 NameDescriptionMinimum SW Version
Public MethodCopyPolynomialTraceToDataRegisterCopy this graph's computed polynomial trace to the specified data register by name.  17.00
Public MethodCopyToCopy this Graph properties to the specified Graph/>.  17.00
Public MethodCreateObjRefCreates an object that contains all the relevant information required to generate a proxy used to communicate with a remote object. (Inherited from System.MarshalByRefObject)—
Public MethodForceRebuildKeyMapThis method is used to force a refresh of the key map. This is necessary in cases where the key mappings to the API objects change. This can happen when the index of an item within a collection is reflected in the key name, and an item is removed from the middle of a collection. (Inherited from Agilent.SA.Vsa.RemotableObject)—
Public MethodGetLifetimeServiceRetrieves the current lifetime service object that controls the lifetime policy for this instance. (Inherited from System.MarshalByRefObject)—
Public MethodInitializeLifetimeServiceObtains a lifetime service object to control the lifetime policy for this instance. (Inherited from Agilent.SA.Vsa.RemotableObject)—
‡ This is the minimum 89600 VSA software version level needed to use this member.
Top

Public Events

 NameDescriptionMinimum SW Version
Public EventPropertyChangedOccurs when a property value changes. (Inherited from Agilent.SA.Vsa.RemotableObject)—
Public EventPropertyInfoChangedOccurs when secondary information about a property, such as limits, changes. (Inherited from Agilent.SA.Vsa.RemotableObject)—
Public EventRemotePropertyChangedOccurs when a property value changes. (Inherited from Agilent.SA.Vsa.RemotableObject)—
Public EventRemotePropertyInfoChangedOccurs when secondary information about a property, such as limits, changes. (Inherited from Agilent.SA.Vsa.RemotableObject)14.00
‡ This is the minimum 89600 VSA software version level needed to use this member.
Top

See Also