| Visual Basic (Declaration) | |
|---|---|
Public MustOverride Property AverageCount As Integer | |
| C# | |
|---|---|
public abstract int AverageCount {get; set;} | |
The IQ Noise Correction procedure will acquire multiple repetitions of the signal and average them together as part of correcting the analyzer noise contribution. This parameter indicates the number of repetitions to average. More averages will improve the measurement accuracy but will also increase the amount of data acquired and the time needed to process it.
Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)