Keysight 89600 VSA .NET API
IQNoiseCorrection Class Members
See Also  Properties  Methods  Events
Agilent.SA.Vsa.Interfaces Assembly > Agilent.SA.Vsa Namespace : IQNoiseCorrection Class

Glossary Item Box

The following tables list the members exposed by IQNoiseCorrection.

Public Properties

 NameDescriptionMinimum SW Version
Public PropertyAverageCountGets or sets the number of averages to use for reducing the effective contribution of the analyzer noise to the resulting noise-corrected IQ data.  —
Public PropertyCurrentNoiseMeasurementOperationGets the current manual noise measurement operation.  30.00
Public PropertyEnabledGets or sets a value indicating whether IQ noise correction is enabled.  —
Public PropertyIsDisposedGets a value indicating whether the object has been disposed. If an object has been disposed any attempt to use it will lead to an ObjectDisposedException being thrown. (Inherited from Agilent.SA.Vsa.RemotableObject)—
Public PropertyKtbNoiseRemovedGets or sets a value indicating whether to remove kTB noise when Mode=IQNoiseCorrectionMode.UncorrelatedAnalyzerNoise.  29.40
Public PropertyManualNoiseProfileEnabledGets or sets a value indicating whether to use a custom noise profile when Input.DataFrom==DataSource.Hardware.  30.00
Public PropertyModeGets or sets the noise sources for which to correct.  29.40
Public PropertyRepetitionAutoDetectedGets or sets a value indicating whether the repetition period of the signal is automatically determined.  —
Public PropertyRepetitionGuidanceGets or sets the repetition period (or max repetition period) of the signal being measured in seconds.  —
Public PropertyRepetitionGuidanceInSamplesGets or sets the RepetitionGuidance parameter in terms of samples at the Raw Main Time sample rate.  29.40
Public PropertySignalDefinitionAutoGets or sets a value indicating whether to automatically update the noise correction parameters using the values provided by the current Measurement.MeasurementExtensionType.  —
Public PropertySignalModeGets or sets a value indicating the type of signal being measured.  —
Public PropertyTemperatureGets or sets the temperature in Kelvin used for the KTB noise floor calculation.  29.40
Public PropertyTimeTrackingEnabledGets or sets a value indicating whether time tracking (fine time alignment between repetitions) is performed before coherent averaging.  29.40
‡ This is the minimum 89600 VSA software version level needed to use this member.
Top

Public Methods

 NameDescriptionMinimum SW Version
Public MethodCreateObjRefCreates an object that contains all the relevant information required to generate a proxy used to communicate with a remote object. (Inherited from System.MarshalByRefObject)—
Public MethodExportManualNoiseProfileExports a custom noise profile to the specified file.  30.00
Public MethodForceRebuildKeyMapThis method is used to force a refresh of the key map. This is necessary in cases where the key mappings to the API objects change. This can happen when the index of an item within a collection is reflected in the key name, and an item is removed from the middle of a collection. (Inherited from Agilent.SA.Vsa.RemotableObject)—
Public MethodGetLifetimeServiceRetrieves the current lifetime service object that controls the lifetime policy for this instance. (Inherited from System.MarshalByRefObject)—
Public MethodImportManualNoiseProfileImports a custom noise profile from the specified file.  30.00
Public MethodInitializeLifetimeServiceObtains a lifetime service object to control the lifetime policy for this instance. (Inherited from Agilent.SA.Vsa.RemotableObject)—
Public MethodStartNoiseMeasurementStarts a procedure to measure the noise profile of the current hardware setup (for Manual Noise Profile mode).  30.00
‡ This is the minimum 89600 VSA software version level needed to use this member.
Top

Public Events

 NameDescriptionMinimum SW Version
Public EventPropertyChangedOccurs when a property value changes. (Inherited from Agilent.SA.Vsa.RemotableObject)—
Public EventPropertyInfoChangedOccurs when secondary information about a property, such as limits, changes. (Inherited from Agilent.SA.Vsa.RemotableObject)—
Public EventRemotePropertyChangedOccurs when a property value changes. (Inherited from Agilent.SA.Vsa.RemotableObject)—
Public EventRemotePropertyInfoChangedOccurs when secondary information about a property, such as limits, changes. (Inherited from Agilent.SA.Vsa.RemotableObject)14.00
‡ This is the minimum 89600 VSA software version level needed to use this member.
Top

See Also