| Visual Basic (Declaration) | |
|---|---|
Public Overridable Sub ImportManualNoiseProfile( _ ByVal filePath As String _ ) | |
Parameters
- filePath
- path to a .mat file in the format saved by ExportManualNoiseProfile
Note, the noise profile should exactly match the measurement state of the I/Q acquisition for the IQNC measurement currently being performed. In addition, the hardware should also be in the same state (this is not known by VSA and is the user's responsibility). If the noise profile does not match the current I/Q measurement state (center, span, HW extension parameters, etc.), the IQNC measurement may not be valid.
Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)
Minimum Software Version Requirement: Keysight 89600 VSA Ver 30.00