Keysight 89600 VSA .NET API
InputChannel Class
Members  See Also 
Agilent.SA.Vsa.Interfaces Assembly > Agilent.SA.Vsa Namespace : InputChannel Class


Glossary Item Box

Implements an input channel. Represents an input channel.

Object Model

InputChannel ClassChannelId Structure

Syntax

Visual Basic (Declaration) 
Public MustInherit Class InputChannel 
   Inherits RemotableObject
   Implements IPropertyInfo, IPropertyInfo2, IRemoteNotifyPropertyChanged, IRemoteNotifyPropertyInfoChanged 
C++/CLI 
public ref class InputChannel abstract : public RemotableObject, IPropertyInfo, IPropertyInfo2, IRemoteNotifyPropertyChanged, IRemoteNotifyPropertyInfoChanged  

Remarks

All input channel objects derive from this InputChannel class. The AnalogChannel and DigitalChannel classes are used for properties specific to those types of channels.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also