Keysight Pathwave 89600 VSA .NET API
InputExtension Class Methods
See Also 
Agilent.SA.Vsa.Interfaces Assembly > Agilent.SA.Vsa Namespace : InputExtension Class


Glossary Item Box

For a list of all members of this type, see InputExtension members.

Public Methods

 NameDescriptionMinimum SW Version
Public MethodCreateObjRefCreates an object that contains all the relevant information required to generate a proxy used to communicate with a remote object. (Inherited from System.MarshalByRefObject)
Public MethodForceRebuildKeyMapThis method is used to force a refresh of the key map. This is necessary in cases where the key mappings to the API objects change. This can happen when the index of an item within a collection is reflected in the key name, and an item is removed from the middle of a collection. (Inherited from Agilent.SA.Vsa.RemotableObject)
Public MethodGetLifetimeServiceRetrieves the current lifetime service object that controls the lifetime policy for this instance. (Inherited from System.MarshalByRefObject)
Public MethodGetParameterGets the value of the named parameter on the specified instrument type.  
Public MethodInitializeLifetimeServiceObtains a lifetime service object to control the lifetime policy for this instance. (Inherited from Agilent.SA.Vsa.RemotableObject)
Public MethodParameterNamesGets an array of strings representing the named parameters that can be configured on this hardware.  
Public MethodSetParameterSets the named parameter on the specified instrument type to the value specified.  
‡ This is the minimum 89600 VSA software version level needed to use this member.
Top

See Also