Keysight 89600 VSA .NET API
GroupIndex Property
See Also 
Agilent.SA.Vsa.Interfaces Assembly > Agilent.SA.Vsa Namespace > InputExtension Class : GroupIndex Property


Glossary Item Box

Gets the index of the instrument group in the current hardware configuration that is associated with this input extension object (for the case when Input.AcquisitionSequenceCount has a value of 1). When the Input.AcquisitionSequenceCount has a value greater than 1 then this property is the index of the InputExtension item within the InputExtensionCollection.

Syntax

Visual Basic (Declaration) 
Public ReadOnly Property GroupIndex As Integer
C# 
public int GroupIndex {get;}
C++/CLI 
public:
property int GroupIndex {
   int get();
}

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also