Keysight 89600 VSA .NET API
InputLogicalChannelCollection Class
Members  See Also 
Agilent.SA.Vsa.Interfaces Assembly > Agilent.SA.Vsa Namespace : InputLogicalChannelCollection Class


Glossary Item Box

Represents a collection of logical input channels.

Object Model

InputLogicalChannelCollection ClassInputLogicalChannel ClassLogicalChannelId Structure

Syntax

Remarks

A logical input channel may be composed of one or more input channels (physical channel). Some parts of the API (such as Frequency.Channels and Input.ChangeLogicalChannels) deal with settings on a per logical channel basis while other parts (like Analog.Channels, etc.) deal with settings on a per input channel (physical channel) basis.

Note: Use the Input.ChangeLogicalChannelsByCount or Input.ChangeLogicalChannels methods to change this collection.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also