Keysight 89600 VSA .NET API
InputTriggerChannel Class
Members  See Also 
Agilent.SA.Vsa.Interfaces Assembly > Agilent.SA.Vsa Namespace : InputTriggerChannel Class


Glossary Item Box

Represents input channel used for trigger properties

Syntax

Visual Basic (Declaration) 
Public MustInherit Class InputTriggerChannel 
   Inherits RemotableObject
   Implements IPropertyInfo, IPropertyInfo2, IRemoteNotifyPropertyChanged, IRemoteNotifyPropertyInfoChanged 
C++/CLI 
public ref class InputTriggerChannel abstract : public RemotableObject, IPropertyInfo, IPropertyInfo2, IRemoteNotifyPropertyChanged, IRemoteNotifyPropertyInfoChanged  

Remarks

The InputTriggerChannel object represents the measurement triggering functionality on an input channel that supports independent properties for each channel (Trigger)/>).

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 27.00

See Also