Keysight 89600 VSA .NET API
LevelHysteresis Property
See Also 
Agilent.SA.Vsa.Interfaces Assembly > Agilent.SA.Vsa Namespace > InputTrigger Class : LevelHysteresis Property


Glossary Item Box

Gets or sets the trigger level hysteresis in dB relative to the trigger level. For a gating trigger the stop gating condition will not be satisfied unless the signal crosses the Trigger Level minus this value (in dB).

Syntax

Visual Basic (Declaration) 
Public Overridable Property LevelHysteresis As Double
C# 
public virtual double LevelHysteresis {get; set;}
C++/CLI 
public:
virtual property double LevelHysteresis {
   double get();
   void set (    double value);
}

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 25.40

See Also