Keysight 89600 VSA .NET API
InputTrigger Class Members
See Also  Properties  Methods  Events
Agilent.SA.Vsa.Interfaces Assembly > Agilent.SA.Vsa Namespace : InputTrigger Class

Glossary Item Box

The following tables list the members exposed by InputTrigger.

Public Properties

 NameDescriptionMinimum SW Version
Public PropertyActualTriggerOutGets the actual current trigger out state. This may vary as a function of other state even though the TriggerOut value is not changed. The TriggerOut value should not be coerced from what was set (as long as it is a supported value) but the actual current value should be reflected here and be TriggerOut.Off, TriggerOut.Unknown, or the current state of TriggerOut.  24.00
Public PropertyChannelGets or sets the input channel that is triggered (by specifying the index of the channel). (Inherited from Agilent.SA.Vsa.Trigger)—
Public PropertyChannelsGets the collection of InputTriggerChannel objects representing per-channel trigger properties that are supported by the hardware and by setup  27.00
Public PropertyDelayGets or sets the trigger delay in seconds. (Inherited from Agilent.SA.Vsa.Trigger)—
Public PropertyExternalLevelGets or sets the external trigger level in volts.  —
Public PropertyFrequencyMaskGets the FrequencyMaskTrigger object for trigger.  17.00
Public PropertyHoldoffGets or sets the trigger holdoff in seconds. (Inherited from Agilent.SA.Vsa.Trigger)—
Public PropertyHoldoffStyleGets or sets the trigger holdoff style. (Inherited from Agilent.SA.Vsa.Trigger)—
Public PropertyIsDisposedGets a value indicating whether the object has been disposed. If an object has been disposed any attempt to use it will lead to an ObjectDisposedException being thrown. (Inherited from Agilent.SA.Vsa.RemotableObject)—
Public PropertyLevelGets or sets the trigger level in volts for the specified input channel. (Inherited from Agilent.SA.Vsa.Trigger)—
Public PropertyLevelHysteresisGets or sets the trigger level hysteresis in dB relative to the trigger level. For a gating trigger the stop gating condition will not be satisfied unless the signal crosses the Trigger Level minus this value (in dB).  25.40
Public PropertyMagnitudeLevelGets or sets the magnitude trigger level for the specified input channel. (Inherited from Agilent.SA.Vsa.Trigger)—
Public PropertyPeriodicOffsetGets or sets the period offset of the periodic trigger timer in seconds. This property is only supported when the PeriodicSyncStyle is set to a value of TriggerStyle.Auto  25.40
Public PropertyPeriodicPeriodGets or sets the period of the periodic trigger timer (in seconds).  —
Public PropertyPeriodicSyncDelayGets or sets the delay between the sync trigger and the periodic trigger timer when the sync occurs.  —
Public PropertyPeriodicSyncStyleGets or sets the source (style) of the periodic sync trigger.  25.40
Public PropertyRFBurstLevelGets or sets the trigger level in dBm for the RF Burst trigger  18.50
Public PropertySlopeGets or sets the trigger slope. (Inherited from Agilent.SA.Vsa.Trigger)—
Public PropertyStopDelayGets or sets the delay between when data for a gated trigger should stop based upon the gating criteria (such as a level) and when it actually stops.  25.40
Public PropertyStyleGets or sets the trigger style. (Inherited from Agilent.SA.Vsa.Trigger)—
Public PropertyTimeQualificationCriteriaGets or sets the time qualification criteria.  19.00
Public PropertyTimeQualificationTime1Gets or sets the lower duration (time1) in seconds for time qualification trigger.  19.00
Public PropertyTimeQualificationTime2Gets or sets the upper duration (time2) in seconds for time qualification trigger.  19.00
Public PropertyTriggerOutGets or sets whether to generate a trigger out when the acquisition occurs and if so what output connector to generate it on. This is the desired trigger out and the actual trigger out state will be reflected in ActualTriggerOut.  24.00
‡ This is the minimum 89600 VSA software version level needed to use this member.
Top

Public Methods

 NameDescriptionMinimum SW Version
Public MethodCreateObjRefCreates an object that contains all the relevant information required to generate a proxy used to communicate with a remote object. (Inherited from System.MarshalByRefObject)—
Public MethodForceRebuildKeyMapThis method is used to force a refresh of the key map. This is necessary in cases where the key mappings to the API objects change. This can happen when the index of an item within a collection is reflected in the key name, and an item is removed from the middle of a collection. (Inherited from Agilent.SA.Vsa.RemotableObject)—
Public MethodGetLifetimeServiceRetrieves the current lifetime service object that controls the lifetime policy for this instance. (Inherited from System.MarshalByRefObject)—
Public MethodInitializeLifetimeServiceObtains a lifetime service object to control the lifetime policy for this instance. (Inherited from Agilent.SA.Vsa.RemotableObject)—
‡ This is the minimum 89600 VSA software version level needed to use this member.
Top

Public Events

 NameDescriptionMinimum SW Version
Public EventPropertyChangedOccurs when a property value changes. (Inherited from Agilent.SA.Vsa.RemotableObject)—
Public EventPropertyInfoChangedOccurs when secondary information about a property, such as limits, changes. (Inherited from Agilent.SA.Vsa.RemotableObject)—
Public EventRemotePropertyChangedOccurs when a property value changes. (Inherited from Agilent.SA.Vsa.RemotableObject)—
Public EventRemotePropertyInfoChangedOccurs when secondary information about a property, such as limits, changes. (Inherited from Agilent.SA.Vsa.RemotableObject)14.00
‡ This is the minimum 89600 VSA software version level needed to use this member.
Top

See Also