Keysight 89600 VSA .NET API
ChangeMeasurementChannels Method
See Also 
Agilent.SA.Vsa.Interfaces Assembly > Agilent.SA.Vsa Namespace > Input Class : ChangeMeasurementChannels Method


Glossary Item Box

Selects which logical channels to use as measurement channels for this measurement.

Overload List

OverloadDescription
ChangeMeasurementChannels(Int32[])Selects which logical channels to use as measurement channels for this measurement.  
ChangeMeasurementChannels(SequentialTrackingMode,Int32[])Selects which logical channels to use as measurement channels for this measurement and what sequential input tracking mode to use.  

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also