| Visual Basic (Declaration) | |
|---|---|
Public Function New( _ ByVal name As String, _ ByVal display As LimitLineDisplay, _ ByVal result As MarkersLimitTestResult, _ ByVal x As Double, _ ByVal y As Double _ ) | |
| C# | |
|---|---|
public LimitResultData( string name, LimitLineDisplay display, MarkersLimitTestResult result, double x, double y ) | |
| C++/CLI | |
|---|---|
public: LimitResultData( String^ name, LimitLineDisplay display, MarkersLimitTestResult result, double x, double y ) | |
Parameters
- name
- The name of the LimitLine.
- display
- Whether this is a limit or a margin.
- result
- The pass/fail status of the LimitLine
- x
- The X-value of the highest Y failure point, or the lowest margin point if LimitLine passed.
- y
- The Y-value of the highest Y failure point, or the lowest margin point if LimitLine passed.
Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)