| Visual Basic (Declaration) | |
|---|---|
Public Overloads Overrides Function Equals( _ ByVal obj As Object _ ) As Boolean | |
Parameters
- obj
- The object to compare with the current instance.
Return Value
true if the specified object has the same Operation and ChannelIds as the current instance; otherwise, false.Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)
Reference
LogicalChannelId StructureLogicalChannelId Members
Overload List
Base Implementation in Equals