For a list of all members of this type, see Macro members.
Name | Description | Minimum SW Version | |
---|---|---|---|
![]() | Build | Initiates a build of the macro. | — |
![]() | CreateObjRef | Creates an object that contains all the relevant information required to generate a proxy used to communicate with a remote object. (Inherited from System.MarshalByRefObject) | — |
![]() | ForceRebuildKeyMap | This method is used to force a refresh of the key map. This is necessary in cases where the key mappings to the API objects change. This can happen when the index of an item within a collection is reflected in the key name, and an item is removed from the middle of a collection. (Inherited from Agilent.SA.Vsa.RemotableObject) | — |
![]() | GetLifetimeService | Retrieves the current lifetime service object that controls the lifetime policy for this instance. (Inherited from System.MarshalByRefObject) | — |
![]() | InitializeLifetimeService | Obtains a lifetime service object to control the lifetime policy for this instance. (Inherited from Agilent.SA.Vsa.RemotableObject) | — |
![]() | Quit | Request the macro to stop running. | — |
![]() | Run | Start the macro running. | — |
‡ This is the minimum 89600 VSA software version level needed to use this member. |