Keysight 89600 VSA .NET API
Marker Class
Members  See Also 
Agilent.SA.Vsa.Interfaces Assembly > Agilent.SA.Vsa Namespace : Marker Class


Glossary Item Box

The Marker class represents one marker on a Trace.

Syntax

Visual Basic (Declaration) 
Public MustInherit Class Marker 
   Inherits RemotableObject
   Implements IPropertyInfo, IPropertyInfo2, IRemoteNotifyPropertyChanged, IRemoteNotifyPropertyInfoChanged 

Remarks

There are properties to control the marker presentation and calculations.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also