Keysight 89600 VSA .NET API
MarkerCollection Class
Members  See Also 
Agilent.SA.Vsa.Interfaces Assembly > Agilent.SA.Vsa Namespace : MarkerCollection Class


Glossary Item Box

The MarkerCollection class contains a collection of Marker objects.

Object Model

MarkerCollection ClassAcpAdjacentChannelCollection ClassAcpAdjacentChannel ClassMarker ClassMarker ClassMarker ClassLimitResultData ClassMarker Class

Syntax

Remarks

In addition, you can set global marker properties from this object, such as the polar format for the markers.

The collection contains a minimum of 1 Marker objects.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also