Keysight 89600 VSA .NET API
AcpReferenceOffsetFreq Property
See Also 
Agilent.SA.Vsa.Interfaces Assembly > Agilent.SA.Vsa Namespace > MarkerCollection Class : AcpReferenceOffsetFreq Property


Glossary Item Box

Gets or sets the offset between the measurement center frequency and the reference carrier frequency.

Syntax

Visual Basic (Declaration) 
Public MustOverride Property AcpReferenceOffsetFreq As Double
C# 
public abstract double AcpReferenceOffsetFreq {get; set;}
C++/CLI 
public:
abstract property double AcpReferenceOffsetFreq {
   double get();
   void set (    double value);
}

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also