Keysight 89600 VSA .NET API
ObwCentroid Property
See Also 
Agilent.SA.Vsa.Interfaces Assembly > Agilent.SA.Vsa Namespace > MarkerCollection Class : ObwCentroid Property


Glossary Item Box

Gets the frequency, in Hz, of the calculated centroid of the occupied band.

Syntax

Visual Basic (Declaration) 
Public MustOverride ReadOnly Property ObwCentroid As Double
C# 
public abstract double ObwCentroid {get;}
C++/CLI 
public:
abstract property double ObwCentroid {
   double get();
}

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also