| Visual Basic (Declaration) | |
|---|---|
Public Overridable Property XDecibelBandwidthThreshold As Double | |
| C# | |
|---|---|
public virtual double XDecibelBandwidthThreshold {get; set;} | |
The signal bandwidth is computed based upon the peak in a frequency domain trace where the peak is the bin with the highest value (interpolation is not currently used to find the peak value so ensure there is enough resolution to the bins in the frequency domain trace for the accuracy desired). Simple linear interpolation is used when finding the locations that first cross the threshold value (relative to the peak value) when they are not exactly on bin. Bins close to DC are ignored in order to still be able to measure signal bandwidths in the presence of a large DC component.
Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)
Minimum Software Version Requirement: Keysight 89600 VSA Ver 29.40