| Visual Basic (Declaration) | |
|---|---|
Public MustOverride ReadOnly Property IQBranch As MarkerIQBranch | |
| C# | |
|---|---|
public abstract MarkerIQBranch IQBranch {get;} | |
| C++/CLI | |
|---|---|
public: abstract property MarkerIQBranch IQBranch { MarkerIQBranch get(); } | |
The 3GPP uplink Code Domain Power measurement result contains both I and Q data which are shown at the same time. This property returns whether the marker is on an I- or a Q-point.
Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)