| Visual Basic (Declaration) | |
|---|---|
Public Overridable Property ReferenceTraceIndex As Integer | |
| C# | |
|---|---|
public virtual int ReferenceTraceIndex {get; set;} | |
Property Value
Default value of -1.This property only applies when Position is MarkerPositionType.Delta. A value less than zero indicates Reference is on the same trace as this marker. A value not matching a valid trace will result in invalid Delta marker result values.
Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)
Minimum Software Version Requirement: Keysight 89600 VSA Ver 25.40