| Visual Basic (Declaration) | |
|---|---|
Public MustOverride ReadOnly Property XAxis As Double | |
| C# | |
|---|---|
public abstract double XAxis {get;} | |
The marker's Point or XData properties determine where the marker is located on the data. The X property returns the calculated X axis value of the data at that point. This value is the same as XData, except if the Format is TraceFormatType.IQ or TraceFormatType.Constellation. The XAxisUnit property contains the unit string for the X axis marker location.
Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)