| Visual Basic (Declaration) | |
|---|---|
Public MustOverride ReadOnly Property ZUnit As String | |
| C# | |
|---|---|
public abstract string ZUnit {get;} | |
The z-axis units are associated with the Z property. The z-axis is used for some OFDM trace data types (e.g. Error Vector Spectrum). The z-axis unit for Error Vector Spectrum can be set with the Trace.DemodTimeUnit property. The z-axis unit for Error Vector Time can be set with the Trace.DemodFreqUnit property.
Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)