Keysight 89600 VSA .NET API
GetRecordingMeasurements Method
See Also 
Agilent.SA.Vsa.Interfaces Assembly > Agilent.SA.Vsa Namespace > MeasurementCollection Class : GetRecordingMeasurements Method


Glossary Item Box

Gets a collection of all the measurements that are recording.

Syntax

Visual Basic (Declaration) 
Public Overridable Function GetRecordingMeasurements() As ReadOnlyCollection(Of Measurement)
C# 
public virtual ReadOnlyCollection<Measurement> GetRecordingMeasurements()
C++/CLI 
public:
virtual ReadOnlyCollection<Measurement^>^ GetRecordingMeasurements(); 

Return Value

The collection of recording measurements. The collection is empty if there are no recording measurements.

Remarks

To stop recordings in progress, use Measurement.Pause() or MeasurementCollection.Pause().

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 15.0

See Also