Keysight 89600 VSA .NET API
MeasurementCollection Class Members
See Also  Properties  Methods  Events
Agilent.SA.Vsa.Interfaces Assembly > Agilent.SA.Vsa Namespace : MeasurementCollection Class

Glossary Item Box

The following tables list the members exposed by MeasurementCollection.

Public Properties

 NameDescriptionMinimum SW Version
Public PropertyAcquisitionGets or sets a value indicating how the timing of measurement data acquisition and measurement result calculations should be related between different measurements.  18.50
Public PropertyCountGets the number of items in the collection. (Inherited from Agilent.SA.Vsa.RemotableCollection<Measurement>)—
Public PropertyIsDisposedGets a value indicating whether the object has been disposed. If an object has been disposed any attempt to use it will lead to an ObjectDisposedException being thrown. (Inherited from Agilent.SA.Vsa.RemotableObject)—
Public PropertyItemOverloaded. Returns a handle to the named measurement.  —
Public PropertySelectedIndexGets or sets the index of the currently selected measurement.  —
Public PropertySelectedItemGets or sets the currently selected measurement.  —
Public PropertySequencedPlaybackModeGets or sets a value indicating how sequenced recording playback is coordinated between measurements.  25.40
‡ This is the minimum 89600 VSA software version level needed to use this member.
Top

Public Methods

 NameDescriptionMinimum SW Version
Public MethodCreateOverloaded. Creates a new vector measurement.  —
Public MethodCreateObjRefCreates an object that contains all the relevant information required to generate a proxy used to communicate with a remote object. (Inherited from System.MarshalByRefObject)—
Public MethodForceRebuildKeyMapThis method is used to force a refresh of the key map. This is necessary in cases where the key mappings to the API objects change. This can happen when the index of an item within a collection is reflected in the key name, and an item is removed from the middle of a collection. (Inherited from Agilent.SA.Vsa.RemotableObject)—
Public MethodGetEnumeratorGets an enumerator for the collection. (Inherited from Agilent.SA.Vsa.RemotableCollection<Measurement>)—
Public MethodGetLifetimeServiceRetrieves the current lifetime service object that controls the lifetime policy for this instance. (Inherited from System.MarshalByRefObject)—
Public MethodGetRecordingMeasurementsGets a collection of all the measurements that are recording.  15.0
Public MethodGetRunningMeasurementsGets a collection of all the measurements that are running.  15.00
Public MethodIndexOfOverloaded. Gets the index location of the specified item within the collection. (Inherited from Agilent.SA.Vsa.RemotableCollection<Measurement>)—
Public MethodInitializeLifetimeServiceObtains a lifetime service object to control the lifetime policy for this instance. (Inherited from Agilent.SA.Vsa.RemotableObject)—
Public MethodPauseOverloaded. Causes the specified measurements to transition to the Paused state.  —
Public MethodPresetPresets the analyzer to a single, vector measurement.  15.00
Public MethodRecordCauses the passed measurements to record.  15.0
Public MethodRemoveRemove a Measurement from the collection.  —
Public MethodRemoveAtRemove a Measurement from the collection.  —
Public MethodResetOverloaded. Causes the passed measurements to transition to the Reset state.  —
Public MethodRestartCauses the passed measurements to restart. The Average count is reset to 0 and the measurements transitions to the Running State.  15.00
Public MethodResumeCauses the passed measurements to transition to the Running state.  15.00
Public MethodWaitForMeasurementsDoneOverloaded. Wait for all of the specified measurements to complete.  —
Public MethodWaitForRecordingsDoneOverloaded. Wait for all of the specified recordings to complete.  —
‡ This is the minimum 89600 VSA software version level needed to use this member.
Top

Public Events

 NameDescriptionMinimum SW Version
Public EventCollectionChangedOccurs when an item is added, removed, changed, moved, or the entire list is refreshed. (Inherited from Agilent.SA.Vsa.RemotableCollection<Measurement>)—
Public EventPropertyChangedOccurs when a property value changes. (Inherited from Agilent.SA.Vsa.RemotableObject)—
Public EventPropertyInfoChangedOccurs when secondary information about a property, such as limits, changes. (Inherited from Agilent.SA.Vsa.RemotableObject)—
Public EventRemoteCollectionChangedOccurs when an item is added, removed, changed, moved, or the entire list is refreshed. (Inherited from Agilent.SA.Vsa.RemotableCollection<Measurement>)14.00
Public EventRemotePropertyChangedOccurs when a property value changes. (Inherited from Agilent.SA.Vsa.RemotableObject)—
Public EventRemotePropertyInfoChangedOccurs when secondary information about a property, such as limits, changes. (Inherited from Agilent.SA.Vsa.RemotableObject)14.00
‡ This is the minimum 89600 VSA software version level needed to use this member.
Top

See Also