Keysight 89600 VSA .NET API
Reset() Method
See Also 
Agilent.SA.Vsa.Interfaces Assembly > Agilent.SA.Vsa Namespace > MeasurementCollection Class > Reset Method : Reset() Method


Glossary Item Box

Reset all of the running measurements.

Syntax

Visual Basic (Declaration) 
Public Overloads Overridable Function Reset() As ReadOnlyCollection(Of Measurement)
C# 
public virtual ReadOnlyCollection<Measurement> Reset()
C++/CLI 
public:
virtual ReadOnlyCollection<Measurement^>^ Reset(); 

Return Value

The collection of previously running measurements. The collection is empty if there were no running measurements.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 15.00

See Also