Causes the passed measurements to restart. The Average count is reset to 0 and the measurements transitions to the Running State.
Syntax
Parameters
- measurements
- The list of measurements to restart.
Exceptions
| Exception | Description |
| System.InvalidOperationException | At least one Measurement in the collection cannot run concurrently with selected measurement (Measurement.IsConcurrent = false). |
Remarks
Requirements
Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)
Minimum Software Version Requirement: Keysight 89600 VSA
Ver 15.00
See Also