Keysight 89600 VSA .NET API
DoubleData Property
See Also 
Agilent.SA.Vsa.Interfaces Assembly > Agilent.SA.Vsa Namespace > MeasurementData Class : DoubleData Property


Glossary Item Box

Gets or sets the Y data points as a double array

Syntax

Visual Basic (Declaration) 
Public MustOverride Property DoubleData As Double()
C# 
public abstract double[] DoubleData {get; set;}
C++/CLI 
public:
abstract property array<double>^ DoubleData {
   array<double>^ get();
   void set (    array<double>^ value);
}

Remarks

FloatData returns the data as a float array.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also