Keysight 89600 VSA .NET API
FloatData Property
See Also 
Agilent.SA.Vsa.Interfaces Assembly > Agilent.SA.Vsa Namespace > MeasurementData Class : FloatData Property


Glossary Item Box

Gets or sets the Y data points as a float array

Syntax

Visual Basic (Declaration) 
Public MustOverride Property FloatData As Single()
C# 
public abstract float[] FloatData {get; set;}
C++/CLI 
public:
abstract property array<float>^ FloatData {
   array<float>^ get();
   void set (    array<float>^ value);
}

Remarks

DoubleData returns the data as a double array.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also