Keysight 89600 VSA .NET API
Status Property
See Also 
Agilent.SA.Vsa.Interfaces Assembly > Agilent.SA.Vsa Namespace > MeasurementData Class : Status Property


Glossary Item Box

Gets the Status of the Data.

Syntax

Visual Basic (Declaration) 
Public MustOverride ReadOnly Property Status As MeasurementDataStatus
C# 
public abstract MeasurementDataStatus Status {get;}
C++/CLI 
public:
abstract property MeasurementDataStatus Status {
   MeasurementDataStatus get();
}

Remarks

Returns the status of the data, which may indicate measurement inaccuracies or error conditions. The returned value is a sum of the MeasurementDataStatus bits.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also