Keysight 89600 VSA .NET API
IsEnabledMeasurementExtension Method
See Also 
Agilent.SA.Vsa.Interfaces Assembly > Agilent.SA.Vsa Namespace > Measurement Class : IsEnabledMeasurementExtension Method


extension
The desired measurement type.

Glossary Item Box

Gets a value indicating whether the specified measurement type is enabled.

Syntax

Visual Basic (Declaration) 
Public MustOverride Function IsEnabledMeasurementExtension( _
   ByVal extension As Type _
) As Boolean
C# 
public abstract bool IsEnabledMeasurementExtension( 
   Type extension
)
C++/CLI 
public:
abstract bool IsEnabledMeasurementExtension( 
   Type^ extension
) 

Parameters

extension
The desired measurement type.

Return Value

Returns true if you can set the current measurement to the passed measurement type. Returns false if calling SetMeasurementExtension for this type will throw an exception.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also