Keysight 89600 VSA .NET API
IsMeasurementDone Property
See Also 
Agilent.SA.Vsa.Interfaces Assembly > Agilent.SA.Vsa Namespace > Measurement Class : IsMeasurementDone Property


Glossary Item Box

Gets a value indicating whether the measurement is complete.

Syntax

Visual Basic (Declaration) 
Public MustOverride ReadOnly Property IsMeasurementDone As Boolean
C# 
public abstract bool IsMeasurementDone {get;}
C++/CLI 
public:
abstract property bool IsMeasurementDone {
   bool get();
}

Remarks

For non-averaged measurements, one cycle is all that is required. For averaged measurements, the average must complete.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also