Keysight 89600 VSA .NET API
IsRecording Property
See Also 
Agilent.SA.Vsa.Interfaces Assembly > Agilent.SA.Vsa Namespace > Measurement Class : IsRecording Property


Glossary Item Box

Gets a value indicating whether the measurement is currently making a recording.

Syntax

Visual Basic (Declaration) 
Public MustOverride ReadOnly Property IsRecording As Boolean
C# 
public abstract bool IsRecording {get;}
C++/CLI 
public:
abstract property bool IsRecording {
   bool get();
}

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also