Keysight 89600 VSA .NET API
MeasurementExtension Property
See Also 
Agilent.SA.Vsa.Interfaces Assembly > Agilent.SA.Vsa Namespace > Measurement Class : MeasurementExtension Property


Glossary Item Box

Gets a handle to the current extension object. The caller must cast it to the appropriate type (indicated by the ExtensionType property) to access members of the object.

Syntax

Visual Basic (Declaration) 
Public MustOverride ReadOnly Property MeasurementExtension As IMeasurementExtension
C# 
public abstract IMeasurementExtension MeasurementExtension {get;}
C++/CLI 
public:
abstract property IMeasurementExtension^ MeasurementExtension {
   IMeasurementExtension^ get();
}

Property Value

A handle to the current demodulation object.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also