Keysight 89600 VSA .NET API
NewChangeGroup Method
See Also 
Agilent.SA.Vsa.Interfaces Assembly > Agilent.SA.Vsa Namespace > Measurement Class : NewChangeGroup Method


Glossary Item Box

Turns off the normal measurement updates that occur after property changes until the System.IDisposable.Dispose method is called on the returned IChangeGroup interface.

Syntax

Visual Basic (Declaration) 
Public MustOverride Function NewChangeGroup() As IChangeGroup
C# 
public abstract IChangeGroup NewChangeGroup()
C++/CLI 
public:
abstract IChangeGroup^ NewChangeGroup(); 

Return Value

An IChangeGroup handle on which System.IDisposable.Dispose must be called to re-enable normal measurement updates.

Remarks

Under normal conditions, every time a property on any object in the VSA object model is changed, a measurement update occurs so that the new property setting is properly reflected in the measurement results. However, when programmatically configuring a measurement, it is desirable to set many properties with only a single measurement update once all have been set.

From the time the handle is obtained until the System.IDisposable.Dispose method on it is called, measurement updates are blocked. The update is performed when the System.IDisposable.Dispose method is called on the returned interface.

In the C# language, the "using" construct can be employed to automatically re-enable updates. The code looks like this: using (IChangeGroup changes = measurement.NewChangeGroup()) { // set all properties here } When the "changes" variable falls out of scope at the end of the "using" block, the System.IDisposable.Dispose method is invoked automatically.

In other languages, it is highly recommended that a "try/finally" construct be employed to guarantee that System.IDisposable.Dispose is called regardless of the outcome of the parameter changes. In C# this would look as follows: IChangeGroup changes = measurement.NewChangeGroup(); try { // set all properties here } finally { if (changes != null) changes.Dispose(); }

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also