Parameters
- fileName
- The path to the setup file to recall. Must be a Keysight 89600 VSA Software setup file (.setx extension) or a Agilent 89601A setup file (.set extension).
This method overwrites parts of the current measurement setup with setup specified in the recalled file. The parts that are overwritten are those which describe the input signal. For example, for Custom OFDM measurements, properties like the OFDM System Sample Rate and the Guard Interval describe the input signal. By comparison, settings which control analysis (for example, Pilot Tracking mode), display (for example, constellation coloring mode), or traces (for example, which traces are displayed and in what configuration) are not modified by this method.
Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)
Minimum Software Version Requirement: Keysight 89600 VSA Ver 21.20