Keysight 89600 VSA .NET API
RecordPercentDone Property
See Also 
Agilent.SA.Vsa.Interfaces Assembly > Agilent.SA.Vsa Namespace > Measurement Class : RecordPercentDone Property


Glossary Item Box

Gets the progress of the current recording (0.0 to 100.0 percent).

Syntax

Visual Basic (Declaration) 
Public MustOverride ReadOnly Property RecordPercentDone As Double
C# 
public abstract double RecordPercentDone {get;}
C++/CLI 
public:
abstract property double RecordPercentDone {
   double get();
}

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also