Keysight 89600 VSA .NET API
SetMeasurementExtension(Type) Method
See Also 
Agilent.SA.Vsa.Interfaces Assembly > Agilent.SA.Vsa Namespace > Measurement Class > SetMeasurementExtension Method : SetMeasurementExtension(Type) Method


measurementType
The desired measurement type.

Glossary Item Box

Changes the current measurement to the indicated type (if necessary) and returns a handle to the extension object.

Syntax

Visual Basic (Declaration) 
Public Overloads MustOverride Function SetMeasurementExtension( _
   ByVal measurementType As Type _
) As Object
C# 
public abstract object SetMeasurementExtension( 
   Type measurementType
)
C++/CLI 
public:
abstract Object^ SetMeasurementExtension( 
   Type^ measurementType
) 

Parameters

measurementType
The desired measurement type.

Return Value

A handle to the requested extension object. If the requested measurement type is not available, an exception is thrown. In this case, the previous measurement type is left unchanged.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also