Keysight 89600 VSA .NET API
WaitForRecordingDone Method
See Also 
Agilent.SA.Vsa.Interfaces Assembly > Agilent.SA.Vsa Namespace > Measurement Class : WaitForRecordingDone Method


Glossary Item Box

Wait 10 seconds for the recording to complete.

Overload List

OverloadDescription
WaitForRecordingDone()Wait 10 seconds for the recording to complete.  
WaitForRecordingDone(Int32)Wait for the recording to complete.  

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also