Keysight 89600 VSA .NET API
NoiseCorrection Class
Members  See Also 
Agilent.SA.Vsa.Interfaces Assembly > Agilent.SA.Vsa Namespace : NoiseCorrection Class


Glossary Item Box

This class and the hierarchy under it are used to define the setup for applying noise corrections to a VSA measurement.

Object Model

NoiseCorrection ClassIQNoiseCorrection ClassOperation ClassOperationInfoMessageCollection ClassOperation ClassOperationInfoMessageCollection Class

Syntax

Visual Basic (Declaration) 
Public MustInherit Class NoiseCorrection 
   Inherits RemotableObject
   Implements IPropertyInfo, IPropertyInfo2, IRemoteNotifyPropertyChanged, IRemoteNotifyPropertyInfoChanged 
C++/CLI 
public ref class NoiseCorrection abstract : public RemotableObject, IPropertyInfo, IPropertyInfo2, IRemoteNotifyPropertyChanged, IRemoteNotifyPropertyInfoChanged  

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 29.00

See Also