Gets or sets a value indicating whether the time reference is automatically chosen. When true then if the recording was made using a time reference of measurement start trigger then it will choose
TimeReference.RecordingTrigger, otherwise it will choose
TimeReference.PlaybackTrigger.
Syntax
| Visual Basic (Declaration) | |
|---|
Public Overridable Property TimeReferenceAuto As Boolean |
| C# | |
|---|
public virtual bool TimeReferenceAuto {get; set;} |
| C++/CLI | |
|---|
public:
virtual property bool TimeReferenceAuto {
bool get();
void set ( bool value);
} |
Requirements
Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)
Minimum Software Version Requirement: Keysight 89600 VSA
Ver 29.00
See Also