Keysight 89600 VSA .NET API
PlaybackTrigger Class Members
See Also  Properties  Methods  Events
Agilent.SA.Vsa.Interfaces Assembly > Agilent.SA.Vsa Namespace : PlaybackTrigger Class

Glossary Item Box

The following tables list the members exposed by PlaybackTrigger.

Public Properties

 NameDescriptionMinimum SW Version
Public PropertyChannelGets or sets the input channel that is triggered (by specifying the index of the channel). (Inherited from Agilent.SA.Vsa.Trigger)—
Public PropertyDelayGets or sets the trigger delay in seconds. (Inherited from Agilent.SA.Vsa.Trigger)—
Public PropertyHoldoffGets or sets the trigger holdoff in seconds. (Inherited from Agilent.SA.Vsa.Trigger)—
Public PropertyHoldoffStyleGets or sets the trigger holdoff style. (Inherited from Agilent.SA.Vsa.Trigger)—
Public PropertyIsDisposedGets a value indicating whether the object has been disposed. If an object has been disposed any attempt to use it will lead to an ObjectDisposedException being thrown. (Inherited from Agilent.SA.Vsa.RemotableObject)—
Public PropertyLevelGets or sets the trigger level in volts for the specified input channel. (Inherited from Agilent.SA.Vsa.Trigger)—
Public PropertyMagnitudeLevelGets or sets the magnitude trigger level for the specified input channel. (Inherited from Agilent.SA.Vsa.Trigger)—
Public PropertyPeriodicOffsetGets or sets the period offset of the periodic trigger timer in seconds. This property is only supported when the PeriodicSyncStyle is set to a value of TriggerStyle.Auto. The default value is 0 seconds.  29.00
Public PropertyPeriodicPeriodGets or sets the period of the periodic trigger timer (in seconds). The default value is 10 milliseconds.  29.00
Public PropertyPeriodicSyncDelayGets or sets the delay in seconds between the sync trigger and the periodic trigger timer when the sync occurs. The default value is 0 seconds.  29.00
Public PropertyPeriodicSyncStyleGets or sets the source (style) of the periodic sync trigger.  29.00
Public PropertySlopeGets or sets the trigger slope. (Inherited from Agilent.SA.Vsa.Trigger)—
Public PropertyStyleGets or sets the trigger style. (Inherited from Agilent.SA.Vsa.Trigger)—
Public PropertyTimeReferenceGets or sets the time reference for playback. This is what the T=0 location is and what time axis times are relative to during playback.  29.00
Public PropertyTimeReferenceAutoGets or sets a value indicating whether the time reference is automatically chosen. When true then if the recording was made using a time reference of measurement start trigger then it will choose TimeReference.RecordingTrigger, otherwise it will choose TimeReference.PlaybackTrigger.  29.00
‡ This is the minimum 89600 VSA software version level needed to use this member.
Top

Public Methods

 NameDescriptionMinimum SW Version
Public MethodCreateObjRefCreates an object that contains all the relevant information required to generate a proxy used to communicate with a remote object. (Inherited from System.MarshalByRefObject)—
Public MethodForceRebuildKeyMapThis method is used to force a refresh of the key map. This is necessary in cases where the key mappings to the API objects change. This can happen when the index of an item within a collection is reflected in the key name, and an item is removed from the middle of a collection. (Inherited from Agilent.SA.Vsa.RemotableObject)—
Public MethodGetLifetimeServiceRetrieves the current lifetime service object that controls the lifetime policy for this instance. (Inherited from System.MarshalByRefObject)—
Public MethodInitializeLifetimeServiceObtains a lifetime service object to control the lifetime policy for this instance. (Inherited from Agilent.SA.Vsa.RemotableObject)—
‡ This is the minimum 89600 VSA software version level needed to use this member.
Top

Public Events

 NameDescriptionMinimum SW Version
Public EventPropertyChangedOccurs when a property value changes. (Inherited from Agilent.SA.Vsa.RemotableObject)—
Public EventPropertyInfoChangedOccurs when secondary information about a property, such as limits, changes. (Inherited from Agilent.SA.Vsa.RemotableObject)—
Public EventRemotePropertyChangedOccurs when a property value changes. (Inherited from Agilent.SA.Vsa.RemotableObject)—
Public EventRemotePropertyInfoChangedOccurs when secondary information about a property, such as limits, changes. (Inherited from Agilent.SA.Vsa.RemotableObject)14.00
‡ This is the minimum 89600 VSA software version level needed to use this member.
Top

See Also