Keysight 89600 VSA .NET API
AreCorrectionConstantsEnabled Property
See Also 
Agilent.SA.Vsa.Interfaces Assembly > Agilent.SA.Vsa Namespace > PlaybackUserCorrectionChannel Class : AreCorrectionConstantsEnabled Property


Glossary Item Box

Gets or sets a value indicating whether fixed calibration constants (Gain, Delay, DcOffset) are used to correct the measurement.

Syntax

Visual Basic (Declaration) 
Public MustOverride Property AreCorrectionConstantsEnabled As Boolean
C# 
public abstract bool AreCorrectionConstantsEnabled {get; set;}
C++/CLI 
public:
abstract property bool AreCorrectionConstantsEnabled {
   bool get();
   void set (    bool value);
}

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also