Keysight 89600 VSA .NET API
PlaybackUserCorrectionChannel Class Members
See Also  Properties  Methods  Events
Agilent.SA.Vsa.Interfaces Assembly > Agilent.SA.Vsa Namespace : PlaybackUserCorrectionChannel Class

Glossary Item Box

The following tables list the members exposed by PlaybackUserCorrectionChannel.

Public Properties

 NameDescriptionMinimum SW Version
Public PropertyAreCorrectionConstantsEnabledGets or sets a value indicating whether fixed calibration constants (Gain, Delay, DcOffset) are used to correct the measurement.  —
Public PropertyDCOffsetGets or sets the DC offset added (in Volts) to an input channel.  —
Public PropertyDelayGets or sets the time delay added (in Sec) to the specified input channel.  —
Public PropertyGainGets or sets the gain multiplier (in V/V) applied to the specified input channel.  —
Public PropertyIFExternalCalibrationFileGets or sets the file which contains the external IF calibration data.  —
Public PropertyIsDisposedGets a value indicating whether the object has been disposed. If an object has been disposed any attempt to use it will lead to an ObjectDisposedException being thrown. (Inherited from Agilent.SA.Vsa.RemotableObject)—
Public PropertyIsIFExternalCorrectionEnabledGets or sets a value indicating whether the calibration data in IFExternalCalibrationFile is used to correct the input data.  —
Public PropertyIsRFExternalCorrectionEnabledGets or sets a value indicating whether the calibration data in RFExternalCalibrationFile is used to correct the input data.  —
Public PropertyPhaseOffsetGets or sets a value indicating the phase offset used to correct the measurement  —
Public PropertyRFExternalCalibrationFilesGets the collection of files which contains the external RF calibration data.  —
‡ This is the minimum 89600 VSA software version level needed to use this member.
Top

Public Methods

 NameDescriptionMinimum SW Version
Public MethodCreateObjRefCreates an object that contains all the relevant information required to generate a proxy used to communicate with a remote object. (Inherited from System.MarshalByRefObject)—
Public MethodForceRebuildKeyMapThis method is used to force a refresh of the key map. This is necessary in cases where the key mappings to the API objects change. This can happen when the index of an item within a collection is reflected in the key name, and an item is removed from the middle of a collection. (Inherited from Agilent.SA.Vsa.RemotableObject)—
Public MethodGetLifetimeServiceRetrieves the current lifetime service object that controls the lifetime policy for this instance. (Inherited from System.MarshalByRefObject)—
Public MethodInitializeLifetimeServiceObtains a lifetime service object to control the lifetime policy for this instance. (Inherited from Agilent.SA.Vsa.RemotableObject)—
‡ This is the minimum 89600 VSA software version level needed to use this member.
Top

Public Events

 NameDescriptionMinimum SW Version
Public EventPropertyChangedOccurs when a property value changes. (Inherited from Agilent.SA.Vsa.RemotableObject)—
Public EventPropertyInfoChangedOccurs when secondary information about a property, such as limits, changes. (Inherited from Agilent.SA.Vsa.RemotableObject)—
Public EventRemotePropertyChangedOccurs when a property value changes. (Inherited from Agilent.SA.Vsa.RemotableObject)—
Public EventRemotePropertyInfoChangedOccurs when secondary information about a property, such as limits, changes. (Inherited from Agilent.SA.Vsa.RemotableObject)14.00
‡ This is the minimum 89600 VSA software version level needed to use this member.
Top

See Also