Keysight 89600 VSA .NET API
ValidateRegister Method
See Also 
Agilent.SA.Vsa.Interfaces Assembly > Agilent.SA.Vsa Namespace > PlaybackUserCorrectionLogicalChannel Class : ValidateRegister Method


dataRegister
The register to validate.

Glossary Item Box

Used to check if a data register can be used for fixed equalization.

Syntax

Visual Basic (Declaration) 
Public MustOverride Function ValidateRegister( _
   ByVal dataRegister As DataRegister _
) As FixedEqualizationValid
C# 
public abstract FixedEqualizationValid ValidateRegister( 
   DataRegister dataRegister
)
C++/CLI 
public:
abstract FixedEqualizationValid ValidateRegister( 
   DataRegister^ dataRegister
) 

Parameters

dataRegister
The register to validate.

Return Value

an enumeration that indicates "valid" or the reason why the specified data is not valid for fixed equalization.

Remarks

Only data registers containing frequency-domain data can be used for fixed equalization.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also