Keysight 89600 VSA .NET API
DefaultPriorityAfterMeasure Field
See Also 
Agilent.SA.Vsa.Interfaces Assembly > Agilent.SA.Vsa Namespace > ProcessingExtension Class : DefaultPriorityAfterMeasure Field


Glossary Item Box

Default priority to use if the processing extension's CustomStep(s) are AfterMeasure.

Syntax

Visual Basic (Declaration) 
Public Const DefaultPriorityAfterMeasure As Integer
C# 
public const int DefaultPriorityAfterMeasure
C++/CLI 
public:
const int DefaultPriorityAfterMeasure

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also