Keysight 89600 VSA .NET API
ProcessingExtension Class Members
See Also  Fields  Properties  Methods  Events
Agilent.SA.Vsa.Interfaces Assembly > Agilent.SA.Vsa Namespace : ProcessingExtension Class

Glossary Item Box

The following tables list the members exposed by ProcessingExtension.

Public Fields

 NameDescriptionMinimum SW Version
Public FieldDefaultPriorityAfterAcquireDefault priority to use if the processing extension's CustomStep(s) are AfterAcquire.  —
Public FieldDefaultPriorityAfterMeasureDefault priority to use if the processing extension's CustomStep(s) are AfterMeasure.  —
Public FieldDefaultPriorityInputNamesDefault priority to use if the processing extension's CustomStep(s) are AtInputNames.  —
‡ This is the minimum 89600 VSA software version level needed to use this member.
Top

Public Properties

 NameDescriptionMinimum SW Version
Public PropertyEnabledGets a value indicating whether the extension is enabled.  —
Public PropertyIsDisposedGets a value indicating whether the object has been disposed. If an object has been disposed any attempt to use it will lead to an ObjectDisposedException being thrown. (Inherited from Agilent.SA.Vsa.RemotableObject)—
Public PropertyNameGets the name of the extension.  16.00
Public PropertyRunMethodErrorGets error message from last call to ExecuteMethod  20.00
‡ This is the minimum 89600 VSA software version level needed to use this member.
Top

Public Methods

 NameDescriptionMinimum SW Version
Public MethodCreateObjRefCreates an object that contains all the relevant information required to generate a proxy used to communicate with a remote object. (Inherited from System.MarshalByRefObject)—
Public MethodForceRebuildKeyMapThis method is used to force a refresh of the key map. This is necessary in cases where the key mappings to the API objects change. This can happen when the index of an item within a collection is reflected in the key name, and an item is removed from the middle of a collection. (Inherited from Agilent.SA.Vsa.RemotableObject)—
Public MethodGetLifetimeServiceRetrieves the current lifetime service object that controls the lifetime policy for this instance. (Inherited from System.MarshalByRefObject)—
Public MethodGetPropertyValueGets the value associated with a public property.  20.00
Public MethodInitializeLifetimeServiceObtains a lifetime service object to control the lifetime policy for this instance. (Inherited from Agilent.SA.Vsa.RemotableObject)—
Public MethodMethodNamesGets an array of the valid method names.  20.00
Public MethodPropertyNamesGets an array of the valid property names.  20.00
Public MethodRunMethodExecute a method  20.00
Public MethodSetPropertyValueSet a property value by name.  20.00
‡ This is the minimum 89600 VSA software version level needed to use this member.
Top

Public Events

 NameDescriptionMinimum SW Version
Public EventPropertyChangedOccurs when a property value changes. (Inherited from Agilent.SA.Vsa.RemotableObject)—
Public EventPropertyInfoChangedOccurs when secondary information about a property, such as limits, changes. (Inherited from Agilent.SA.Vsa.RemotableObject)—
Public EventRemotePropertyChangedOccurs when a property value changes. (Inherited from Agilent.SA.Vsa.RemotableObject)—
Public EventRemotePropertyInfoChangedOccurs when secondary information about a property, such as limits, changes. (Inherited from Agilent.SA.Vsa.RemotableObject)14.00
‡ This is the minimum 89600 VSA software version level needed to use this member.
Top

See Also